ACTION#.SOURCEPARAM
Description
ACTION#.SOURCEPARAM is used to configure an action source. Most sources do not require this parameter. For those sources, ACTION#.SOURCEPARAM is marked NotInUse.
For sources that do require this parameter, ACTION#.SOURCE must be set before ACTION#.SOURCEPARAM. When ACTION#.SOURCE is set, the units, range, and default value of ACTION#.SOURCEPARAM are updated, and the parameter is set to its default value.
Example
This example sets up a move complete action source for motion task 7 on axis 2.
>> ACTION1.SOURCE = 10 (Move complete) >> ACTION1.SOURCEID = 2 (Axis 2) >> ACTION1.SOURCEPARAM = 7 (Motion task 7)
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-01-02-000 |
|
General Information
Type |
Read/Write |
Description | Action source configuration parameter |
Units |
Depends on ACTION#.SOURCE |
Range |
Depends on ACTION#.SOURCE |
Default Value |
Depends on ACTION#.SOURCE |
Data Type |
Float |
See Also | ACTION#.SOURCE, ACTION#.SOURCEID |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
ACTION1.SOURCEPARAM |
3906h |
01h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION2.SOURCEPARAM |
3906h |
02h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION3.SOURCEPARAM |
3906h |
03h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION4.SOURCEPARAM |
3906h |
04h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION5.SOURCEPARAM |
3906h |
05h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION6.SOURCEPARAM |
3906h |
06h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION7.SOURCEPARAM |
3906h |
07h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION8.SOURCEPARAM |
3906h |
08h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION9.SOURCEPARAM |
3906h |
09h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION10.SOURCEPARAM |
3906h |
0ah |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION11.SOURCEPARAM |
3906h |
0bh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION12.SOURCEPARAM |
3906h |
0ch |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION13.SOURCEPARAM |
3906h |
0dh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION14.SOURCEPARAM |
3906h |
0eh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION15.SOURCEPARAM |
3906h |
0fh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION16.SOURCEPARAM |
3906h |
10h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION17.SOURCEPARAM |
3906h |
11h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION18.SOURCEPARAM |
3906h |
12h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION19.SOURCEPARAM |
3906h |
13h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION20.SOURCEPARAM |
3906h |
14h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION21.SOURCEPARAM |
3906h |
15h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION22.SOURCEPARAM |
3906h |
16h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION23.SOURCEPARAM |
3906h |
17h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION24.SOURCEPARAM |
3906h |
18h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION25.SOURCEPARAM |
3906h |
19h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION26.SOURCEPARAM |
3906h |
1ah |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION27.SOURCEPARAM |
3906h |
1bh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION28.SOURCEPARAM |
3906h |
1ch |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION29.SOURCEPARAM |
3906h |
1dh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION30.SOURCEPARAM |
3906h |
1eh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION31.SOURCEPARAM |
3906h |
1fh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION32.SOURCEPARAM |
3906h |
20h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
ACTION1.SOURCEPARAM |
40700 |
9EFC |
Signed32 |
Read/Write |
- |
ACTION2.SOURCEPARAM |
40701 |
9EFD |
Signed32 |
Read/Write |
- |
ACTION3.SOURCEPARAM |
40702 |
9EFE |
Signed32 |
Read/Write |
- |
ACTION4.SOURCEPARAM |
40703 |
9EFF |
Signed32 |
Read/Write |
- |
ACTION5.SOURCEPARAM |
40704 |
9F00 |
Signed32 |
Read/Write |
- |
ACTION6.SOURCEPARAM |
40705 |
9F01 |
Signed32 |
Read/Write |
- |
ACTION7.SOURCEPARAM |
40706 |
9F02 |
Signed32 |
Read/Write |
- |
ACTION8.SOURCEPARAM |
40707 |
9F03 |
Signed32 |
Read/Write |
- |
ACTION9.SOURCEPARAM |
40708 |
9F04 |
Signed32 |
Read/Write |
- |
ACTION10.SOURCEPARAM |
40709 |
9F05 |
Signed32 |
Read/Write |
- |
ACTION11.SOURCEPARAM |
40710 |
9F06 |
Signed32 |
Read/Write |
- |
ACTION12.SOURCEPARAM |
40711 |
9F07 |
Signed32 |
Read/Write |
- |
ACTION13.SOURCEPARAM |
40712 |
9F08 |
Signed32 |
Read/Write |
- |
ACTION14.SOURCEPARAM |
40713 |
9F09 |
Signed32 |
Read/Write |
- |
ACTION15.SOURCEPARAM |
40714 |
9F0A |
Signed32 |
Read/Write |
- |
ACTION16.SOURCEPARAM |
40715 |
9F0B |
Signed32 |
Read/Write |
- |
ACTION17.SOURCEPARAM |
40716 |
9F0C |
Signed32 |
Read/Write |
- |
ACTION18.SOURCEPARAM |
40717 |
9F0D |
Signed32 |
Read/Write |
- |
ACTION19.SOURCEPARAM |
40718 |
9F0E |
Signed32 |
Read/Write |
- |
ACTION20.SOURCEPARAM |
40719 |
9F0F |
Signed32 |
Read/Write |
- |
ACTION21.SOURCEPARAM |
40720 |
9F10 |
Signed32 |
Read/Write |
- |
ACTION22.SOURCEPARAM |
40721 |
9F11 |
Signed32 |
Read/Write |
- |
ACTION23.SOURCEPARAM |
40722 |
9F12 |
Signed32 |
Read/Write |
- |
ACTION24.SOURCEPARAM |
40723 |
9F13 |
Signed32 |
Read/Write |
- |
ACTION25.SOURCEPARAM |
40724 |
9F14 |
Signed32 |
Read/Write |
- |
ACTION26.SOURCEPARAM |
40725 |
9F15 |
Signed32 |
Read/Write |
- |
ACTION27.SOURCEPARAM |
40726 |
9F16 |
Signed32 |
Read/Write |
- |
ACTION28.SOURCEPARAM |
40727 |
9F17 |
Signed32 |
Read/Write |
- |
ACTION29.SOURCEPARAM |
40728 |
9F18 |
Signed32 |
Read/Write |
- |
ACTION30.SOURCEPARAM |
40729 |
9F19 |
Signed32 |
Read/Write |
- |
ACTION31.SOURCEPARAM |
40730 |
9F1A |
Signed32 |
Read/Write |
- |
ACTION32.SOURCEPARAM |
40731 |
9F1B |
Signed32 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
ACTION1.SOURCEPARAM |
40700 |
Float |
Read/Write |
- |
ACTION2.SOURCEPARAM |
40701 |
Float |
Read/Write |
- |
ACTION3.SOURCEPARAM |
40702 |
Float |
Read/Write |
- |
ACTION4.SOURCEPARAM |
40703 |
Float |
Read/Write |
- |
ACTION5.SOURCEPARAM |
40704 |
Float |
Read/Write |
- |
ACTION6.SOURCEPARAM |
40705 |
Float |
Read/Write |
- |
ACTION7.SOURCEPARAM |
40706 |
Float |
Read/Write |
- |
ACTION8.SOURCEPARAM |
40707 |
Float |
Read/Write |
- |
ACTION9.SOURCEPARAM |
40708 |
Float |
Read/Write |
- |
ACTION10.SOURCEPARAM |
40709 |
Float |
Read/Write |
- |
ACTION11.SOURCEPARAM |
40710 |
Float |
Read/Write |
- |
ACTION12.SOURCEPARAM |
40711 |
Float |
Read/Write |
- |
ACTION13.SOURCEPARAM |
40712 |
Float |
Read/Write |
- |
ACTION14.SOURCEPARAM |
40713 |
Float |
Read/Write |
- |
ACTION15.SOURCEPARAM |
40714 |
Float |
Read/Write |
- |
ACTION16.SOURCEPARAM |
40715 |
Float |
Read/Write |
- |
ACTION17.SOURCEPARAM |
40716 |
Float |
Read/Write |
- |
ACTION18.SOURCEPARAM |
40717 |
Float |
Read/Write |
- |
ACTION19.SOURCEPARAM |
40718 |
Float |
Read/Write |
- |
ACTION20.SOURCEPARAM |
40719 |
Float |
Read/Write |
- |
ACTION21.SOURCEPARAM |
40720 |
Float |
Read/Write |
- |
ACTION22.SOURCEPARAM |
40721 |
Float |
Read/Write |
- |
ACTION23.SOURCEPARAM |
40722 |
Float |
Read/Write |
- |
ACTION24.SOURCEPARAM |
40723 |
Float |
Read/Write |
- |
ACTION25.SOURCEPARAM |
40724 |
Float |
Read/Write |
- |
ACTION26.SOURCEPARAM |
40725 |
Float |
Read/Write |
- |
ACTION27.SOURCEPARAM |
40726 |
Float |
Read/Write |
- |
ACTION28.SOURCEPARAM |
40727 |
Float |
Read/Write |
- |
ACTION29.SOURCEPARAM |
40728 |
Float |
Read/Write |
- |
ACTION30.SOURCEPARAM |
40729 |
Float |
Read/Write |
- |
ACTION31.SOURCEPARAM |
40730 |
Float |
Read/Write |
- |
ACTION32.SOURCEPARAM |
40731 |
Float |
Read/Write |
- |